PC Requirements

•Minimum Intel Pentium III CPU 500MHz, 128MB RAM

•USB 1.1 equipped PC; Win2000, WinXP, Vista

•USB 2.0 equipped PC; Win2000, WinXP, Vista

Mac Requirements

•Minimum Apple G4 processor , 128MB RAM

•USB 1.1 equipped Mac; Mac OS 9.2, 10.1.5 or above

•USB 2.0 equipped Mac; Mac OS 10.2 or above

Package Contents

•RAID enclosure X 1

•External Power Adapter; AC Input 100-240V, DC Output +12V/2A, +5V/2A X 1

•Power Cord X 1

•Interface Cables:

•USB2.0 X 1

•Screw Driver X 1

•Accessories pouch (screws) X 1

 

 

PC Requirements

•Minimum Intel Pentium III CPU 500MHz, 128MB RAM

•USB 1.1 equipped PC; Win2000, WinXP, Vista

•USB 2.0 equipped PC; Win2000, WinXP, Vista

•FIREWIRE-1394a equipped PC; Win2000, WinXP, Vista

•FIREWIRE-1394b equipped PC; Win2000, WinXP, Vista

 

Mac Requirements

•Minimum Apple G3 processor (USB or FIREWIRE-1394a / b), 128MB RAM

•USB 1.1 equipped Mac; Mac OS 9.2, 10.1.5 or above

•USB 2.0 equipped Mac; Mac OS 10.2 or above

•FIREWIRE-1394a equipped Mac; Mac OS 9.2, 10.1.5 or above

•FIREWIRE-1394b equipped Mac; Mac OS 10.2 or above

 

 

Package Contents

•RAID enclosure X 1

•External Power Adapter; AC Input 100-240V, DC Output +12V/2A, +5V/2A X 1

•Power Cord X 1

•Interface Cables:

•USB2.0 X 1

•FIREWIRE-1394a (A + A) X 1

•FIREWIRE-1934b (B + B) X 1

•Screw Driver X 1

•Accessories pouch (screws) X 1

 
  PC    ( Microsoft Windows )

 

•Before connecting to the PC please refer to our Hard Drive Assembly procedures for RAID set-up.

 

•If HDD is pre-installed by our vendor, user can plug directly to PC and start using the unit.

If wish to change the setting please refer to Hard Drive Assembly for correctly way of setting.

 

• Turn on PC and start Windows.

• Connect (USB or FIREWIRE-1394) HUR1 and turn on the power.

• Windows will search and install drive automatically.

• Open “My Computer” and “external hard drive” will appear.

 

 

Remove the “external hard drive” from PC.

For safe removal of external hard drive, this is to prevent any data lost. Please always follow the correct removal procedure.

1.Click the icon for external hardware in task bar.

 

2.Choose the hard drive wish to remove and confirm it.

  Macintosh

 

Before connecting to the Macintosh please refer to our Hard Drive Assembly procedures for RAID set-up.

If HDD is pre-installed by our vendor, user can plug directly to Macintosh and start using the unit. If wish

to change the setting please refer to Hard Drive Assembly for correctly way of setting.

 

• Turn on Macintosh and start Mac OS.

• Connect (USB or FIREWIRE-1394) HUR1 and turn on the power.

• Mac OS will search and install drive automatically.

• External drive will appear on Desk top.

 

Remove the “external hard drive” from Macintosh..

• Drag the external hard drive to trash bin.

• Turn off the power.

 

Note:If user wishes to use HUR1 on both Windows and Mac OS system, we recommend that HDD to be formatted at FAT32. Also, please do the formatting under Windows OS. If formatting is done by Mac OS, Windows might not recognize the drive.

 

Our recommendation of file systems to be formatted on HDD:

Before connecting to the Macintosh please refer to our Hard Drive Assembly procedures for RAID set-up.

 

If HDD is pre-installed by our vendor, user can plug directly to Macintosh and start using the unit. If wish to change the setting please refer into Hard Drive Assembly for correctly way of setting.

 

• Turn on Macintosh and start Mac OS.

• Connect (USB or FIREWIRE-1394) HUR1 and turn on the power.

• Mac OS will search and install drive automatically.

• External drive will appear on Desk top.

 

Remove the “external hard drive” from Macintosh..

• Drag the external hard drive to trash bin.

• Turn off the power.

 

Note: If user wishes to use HUR1 on both Windows and Mac OS system, we recommend that HDD to be formatted at FAT32. Also, please do the formatting under Windows OS. If formatting is done by Mac OS, Windows might not recognize the drive.

Our recommendation of file systems to be formatted on HDD:

• Win2000, Win XP, Vista NTFS

• Mac OS X HFS+ (Mac OS Extended)

• Both Windows and Mac OS FAT32